AXIS#.WS.ARM
Description
This command sets wake and shake to start at the next axis enable. Feedback type is not relevant for this command. If AXIS#.WS.STATE is 0 and the drive is disabled, then AXIS#.WS.STATE will change to 1 after issuing AXIS#.WS.ARM. With this command, wake and shake can be repeated if desired.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.WS.ARM | 0x5013 | 0x9 | UDINT | - | - | wo | False |
| AXIS2.WS.ARM | 0x5113 | 0x9 | UDINT | - | - | wo | False |
|
Copyright © 2018 Kollmorgen |
|